2017-09-09 04:11 AM
I use the cubemx to create the project(cubemx 4.22 and stm32CubeF4 1.16),it always occurs FIFO Error Interrupt,when I use dma to write sdio. And It stopes.,when write serveral times.But there is no sdio error interrupt happened.
This is my dma configtion:
/* SDIO DMA Init */
/* SDIO_RX Init */ hdma_sdio_rx.Instance = DMA2_Stream3; hdma_sdio_rx.Init.Channel = DMA_CHANNEL_4; hdma_sdio_rx.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_sdio_rx.Init.PeriphInc = DMA_PINC_DISABLE; hdma_sdio_rx.Init.MemInc = DMA_MINC_ENABLE; hdma_sdio_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; hdma_sdio_rx.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; hdma_sdio_rx.Init.Mode = DMA_PFCTRL; hdma_sdio_rx.Init.Priority = DMA_PRIORITY_VERY_HIGH; hdma_sdio_rx.Init.FIFOMode = DMA_FIFOMODE_ENABLE; hdma_sdio_rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL; hdma_sdio_rx.Init.MemBurst = DMA_MBURST_INC4; hdma_sdio_rx.Init.PeriphBurst = DMA_PBURST_INC4; if (HAL_DMA_Init(&hdma_sdio_rx) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }__HAL_LINKDMA(sdHandle,hdmarx,hdma_sdio_rx);
/* SDIO_TX Init */
hdma_sdio_tx.Instance = DMA2_Stream6; hdma_sdio_tx.Init.Channel = DMA_CHANNEL_4; hdma_sdio_tx.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_sdio_tx.Init.PeriphInc = DMA_PINC_DISABLE; hdma_sdio_tx.Init.MemInc = DMA_MINC_ENABLE; hdma_sdio_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; hdma_sdio_tx.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; hdma_sdio_tx.Init.Mode = DMA_PFCTRL; hdma_sdio_tx.Init.Priority = DMA_PRIORITY_VERY_HIGH; hdma_sdio_tx.Init.FIFOMode = DMA_FIFOMODE_ENABLE; hdma_sdio_tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL; hdma_sdio_tx.Init.MemBurst = DMA_MBURST_INC4; hdma_sdio_tx.Init.PeriphBurst = DMA_PBURST_INC4; if (HAL_DMA_Init(&hdma_sdio_tx) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }__HAL_LINKDMA(sdHandle,hdmatx,hdma_sdio_tx);
/* SDIO interrupt Init */
HAL_NVIC_SetPriority(SDIO_IRQn, 0, 0); HAL_NVIC_EnableIRQ(SDIO_IRQn); /* USER CODE BEGIN SDIO_MspInit 1 */and fatfs driver
/* USER CODE BEGIN BeforeWriteDMABlocksSection */
/* can be used to modify previous code / undefine following code / add code *//* USER CODE END BeforeWriteDMABlocksSection *//** * @brief Writes block(s) to a specified address in an SD card, in DMA mode. * @param pData: Pointer to the buffer that will contain the data to transmit * @param WriteAddr: Address from where data is to be written * @param NumOfBlocks: Number of SD blocks to write * @retval SD status */uint8_t BSP_SD_WriteBlocks_DMA(uint32_t *pData, uint32_t WriteAddr, uint32_t NumOfBlocks){ uint8_t sd_state = MSD_OK; uint8_t *buf = (uint8_t *)pData; uint8_t n; uint32_t timeout = 100000; if ((uint32_t)pData%4!=0) { for(n=0;n<NumOfBlocks;n++){ memcpy(SDIO_DATA_BUFFER,buf,512); /* Write block(s) in DMA transfer mode */ if (HAL_SD_WriteBlocks_DMA(&hsd, (uint8_t *)SDIO_DATA_BUFFER, WriteAddr+512*n, 1) != HAL_OK) { sd_state = MSD_ERROR; } while(SD_TxCplt == 0){ if (timeout -- == 0){ sd_state = MSD_ERROR; break; } } SD_TxCplt = 0; buf += 512; } } else { /* Write block(s) in DMA transfer mode */ if (HAL_SD_WriteBlocks_DMA(&hsd, (uint8_t *)pData, WriteAddr, NumOfBlocks) != HAL_OK) { sd_state = MSD_ERROR; } while(SD_TxCplt == 0){ if (timeout -- == 0){ sd_state = MSD_ERROR; break; } osDelay(4); } SD_TxCplt = 0; } return sd_state; }2018-08-09 06:36 PM