cancel
Showing results for 
Search instead for 
Did you mean: 

Three or one stm32f413 wakeup pin(s) from standby?

Age Zijderveld
Associate II
Posted on September 27, 2017 at 11:17

Dear all,

What are the wakeup pins of the STM32F413VGT? CubeMX and the reference manual says three (PA0/PC0/PC1) but the generated code won't accept PC0 and PC1. And when I write directly into the PWR_CSR register for the two pins, PA0 stops waking up the MCU out of standby. I'm a little bit confused, have I missed an imported part?

Kind regards,

Age

1 ACCEPTED SOLUTION

Accepted Solutions
Age Zijderveld
Associate II
Posted on September 28, 2017 at 02:55

Solved it! The answer is, there are three wake up pins PC0, PC1 and PA1 you can use.

View solution in original post

1 REPLY 1
Age Zijderveld
Associate II
Posted on September 28, 2017 at 02:55

Solved it! The answer is, there are three wake up pins PC0, PC1 and PA1 you can use.