cancel
Showing results for 
Search instead for 
Did you mean: 

Output control Question

Kang Sung Gu
Associate II
Posted on September 18, 2017 at 02:59

0690X00000608HJQAY.png

EX) ODR = 1   -> I/O Pin State = 0 ?

It is True?

If ODR = 1 then I / O port is also 1?

Is it OutputControl Not Gate?

2 REPLIES 2
Posted on September 18, 2017 at 08:22

It's more a block diagram and not a true schematics.

If ODR=1, unless given pin is set to open-drain in OTYPER,  the PMOS is switched on, ie. on output you will see log.1.

If ODR=0, NMOS is switched on ie. output is set to 0.

JW

Posted on September 18, 2017 at 08:53

Thank you for a detailed description