cancel
Showing results for 
Search instead for 
Did you mean: 

CAN Ä° USE PB2 AZ ANY DÄ°O

TARHAN SAMAH
Senior
Posted on January 09, 2018 at 10:06

HELLO because luck of pins we need to use pin PB2 AZ DÄ°O TO READ OR WRÄ°TE, 

Ä°S Ä°T POSSÄ°BLE MXCUBE ACCEPTS THAT BUT DO ANY ONE HAS A Ä°DEA BECAUSE WE ARE DESÄ°GNÄ°NG A PCB WE DONT WANT TAKE A RÄ°SK THAT Ä°T WÄ°LL NOT WORK ,WE COULDNT TEST THAT ON ARDUÄ°NO stm103c8 cart 

THANKS 

2 REPLIES 2
Chris1
Senior III
Posted on January 11, 2018 at 04:13

PB2 can be used as a general-purpose input or output in your application (assumed using an STM32F103). 

However, if you plan to use the embedded boot loader, you should provide a means to pull the pin low (PB2 is also BOOT1) to allow reprogramming the flash memory via USART or USB.

Posted on January 19, 2018 at 12:28

thank you very much copied