cancel
Showing results for 
Search instead for 
Did you mean: 

spirit 1 , and stm32f103xx?

TARHAN SAMAH
Senior
Posted on November 07, 2017 at 09:24

Hello every body we are using stm32f103xx microcontrollers , we want to send our data by wireless using spirit1 module ,

- is it possible ?

-which library is suitable ?

-what about distance amd range of gigahertz modules ?

urgent help needed plz thanks 

Samah Tarhan 

Argebilisim 

1 ACCEPTED SOLUTION

Accepted Solutions
TARHAN SAMAH
Senior
Posted on November 16, 2017 at 12:27

Ä° SOLVE it it was a wrong adapter from hyperterminal to ttl , before i used adm now i use usb dongle ch340g or arduino adapter . now i communicate perfectly with my spirit 1 ,thanks 

View solution in original post

14 REPLIES 14
Andrew Neil
Evangelist
Posted on November 07, 2017 at 10:17

Surely, the answer to this will be found by reading the documentation for this '

spirit1 module'?

You have done that, haven't you ... ?

http://www.8052.com/forum/read/160143

 (it's not by any means new - but it is certainly still applicable!)
Posted on November 07, 2017 at 10:22

Ah - you mean this: 

http://www.st.com/en/wireless-connectivity/spirit1.html

 

Loads of documents on that page for you to read!

Just looking at the very first paragraph of the Dev Kit User Manual:

The kit includes a SPIRIT1 development kit graphical user interface (SPIRIT1 DK - GUI) which allows checking the SPIRIT1 main performance and easily measure parameters such as sensitivity, output power and main features of the SPIRIT1. It also

contains SPIRIT1 firmware libraries for STM32L

and STM8L to allow development of SPIRIT1 applications.
Posted on November 07, 2017 at 10:40

thanks so much mister Andrew ,, so it will not be possible to use on my stm32f103xx series maybe from another libraries  ? , 

-what about transmition range ?? 

also i got another question if we use the STM32ML and wmbus is it free standart or needs fees ? 

Posted on November 07, 2017 at 10:48

yes i mean gıgahertz modules spml1 of st 868 or 915 , i need to establish my network collecting data and send them to pc 

Posted on November 07, 2017 at 12:27

TARHAN SAMAH wrote:

so it will not be possible to use on my stm32f103xx series maybe from another libraries  ? , 

Eh??

:(

What on earth makes you think that??

Posted on November 07, 2017 at 13:18

you mean the sp1ml is usable on stm32f103xx??? can you explain more , i dont understand 

Posted on November 07, 2017 at 14:12

Did you read: 

http://www.8052.com/forum/read/160143

  ?
Posted on November 07, 2017 at 14:34

Might need to be ported. Seem to remember there being a sub-ghz radio on L4 IoT board.

Range tends v to help highly dependent on power, antenna and line of sight.

LoRa which can be used as sub-ghz radio can get 11km LoS without much effort, but about 1km in more obstructed use.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on November 07, 2017 at 17:27

Everything you post to the forum is 'urgent', please read the Hacker FAQ to understand how such requests are interpreted. 

http://www.catb.org/esr/faqs/smart-questions.html#urgent

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..