2017-10-25 02:12 PM
Folks -
Just updated to STM32Cube_FW_L4_V1.10.0 and STM32CubeMX v4.23. I can see the B-L475E-IOT01 discovery board and all its' files in the L4 package. I can also select the STM32L475VGTx MCU from the STM32CubeMX but can NOT see the discovery board. (Would really like to have all the pins pre-configured!) Am I missing something?
cheers,
-jim r
Solved! Go to Solution.
2018-02-19 06:19 AM
Hello,
Please note that the board B-L475E-IOT01A is supported in current version of STM32CubeMX version 4.24 (available since end of January 2018).
Sorry for this delayed notification.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-10-25 02:27 PM
Sorry, forgot to mention this is running on a Mac OSX 10.13.
2017-10-26 01:19 AM
Hi
jim.2435074
,Unfortunately the
B-L475E-IOT01 discovery board isn't yet supported in CubeMX (last version 4.23).
Please apply the workaround suggested in
https://community.st.com/0D70X000006SlG9SAK
witing for its official support un CubeMX.-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-10-26 03:18 AM
Amel -
Thanks for the quick reply! Will do the work-around while waiting. Is the B-L475E-IOT1 going to be incorporated into CubeMX? If so, any guesstimate as to when? Happy to help with beta-testing!
cheers,
-jim r
2018-02-19 06:19 AM
Hello,
Please note that the board B-L475E-IOT01A is supported in current version of STM32CubeMX version 4.24 (available since end of January 2018).
Sorry for this delayed notification.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-03-08 07:40 AM
Amel -
Thanks for the reply. I did notice it when i updated to version 4.24. So far, no problems! Again, thanks for getting back to me.
cheers,
-jim r