cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-1 extended packet length

Adriana Albert
Associate II
Posted on October 05, 2017 at 10:47

I am evaluating the use of the SPBTLE-1S module, based on BlueNRG-1 and Bluetooth v4.2 compilant, to interact with iOS. BLE 4.2 specification includes data length extension feature which improves throughput and reduces transaction time. However, according to documentation, only BlueNRG-2 supports BLE extended packet length feature. 

Is it possible to upgrade BLE stack embedded software (

library managing the RF part

) with a version wich 

extends the possible MTU size up to 158 bytes?

Thank in advance.

1 ACCEPTED SOLUTION

Accepted Solutions
Antonio Vilei
Senior III
Posted on October 09, 2017 at 15:07

Dear Adriana Albert,

as reported in the documentation, only BlueNRG-2 supports the BLE extended packet length and there are no firmware updates available to enable this feature with BlueNRG-1 too.

View solution in original post

1 REPLY 1
Antonio Vilei
Senior III
Posted on October 09, 2017 at 15:07

Dear Adriana Albert,

as reported in the documentation, only BlueNRG-2 supports the BLE extended packet length and there are no firmware updates available to enable this feature with BlueNRG-1 too.