2017-11-15 01:48 AM
Hi,
We are using Tianma’s - TM070RVHG01 TFT in our design with STM32F429 processor working at 168 MHz frequency. We are using EmWin Library on RTX operating system with LTDC support. We are statically storing the required ARGB format in external SDRAM. The data is loaded from SDRAM to LTDC (STM32F4 LCD Controller) using DMA2D and FMC interface (Flexible Memory Controller – Working at 168/2 MHz).
The colour configuration is ARGB8888 and driver configuration of EmWin is GUI_LIN_32.
From datasheet we understand that minimum DCLK is 28 MHz. So we are setting the DCLK as 28 MHz and calculated the parameters for LTDC which are as follows.
From Datasheet
HSYNC Width
20
VSYNC Width
3
HBP
46
VBP
23
Active Width
800
Active Height
480
BVBP
23
HFP
210
VFP
22
Calculated Value for LTDC Register
HSW
19
VSH
2
AHBP
65
AVBP
25
AAW
865
AAH
505
TOTAL W
1075
TOTAL H
527
Issue :
Is there any solution for the above problems without using multi buffer support. Also could you send sample source running on any RTOS for reference
Thanks and Regards,
Manoj
2017-11-30 07:59 AM
Try 180 MHz
2017-11-30 05:32 PM
800*480*60=23Mgz
2018-04-01 07:23 PM
Dear every body,
Chandran.Manoj
Iare using LCD TFT 7 inch 800x480
in our design with STM32F746BTG6processor working at200 MHz frequency.We are usingSTemWinLibrary on RTOS operating system
with LTDCsupport.GUIBuilder.exe software will generate gui data.
I are statically storing the required ARGB format in external SDRAM.
The data is loaded from SDRAM to LTDC (STM32F7 LCD Controller)using DMA2D and FMC interface(Flexible Memory Controller – Working at 200/2 MHz).
Timing LCD TFT 7 inch from datasheet:
http://www.buydisplay.com/download/ic/OTA7001A.pdf
About frequency in system:
- SDRAM: 100MHz, use same bus data 16bit with other device. Examples:nor flash.
/* Timing configuration for 100Mhz as SD clock frequency (System clock is up to 200Mhz) */
Timing.LoadToActiveDelay = 2; Timing.ExitSelfRefreshDelay = 7; Timing.SelfRefreshTime = 4; Timing.RowCycleDelay = 7; Timing.WriteRecoveryTime = 2; Timing.RPDelay = 2; Timing.RCDDelay = 2; sdramHandle.Init.SDBank = FMC_SDRAM_BANK1;sdramHandle.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_9;
sdramHandle.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_13;sdramHandle.Init.MemoryDataWidth = SDRAM_MEMORY_WIDTH;
sdramHandle.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4; sdramHandle.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_2; sdramHandle.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE; sdramHandle.Init.SDClockPeriod = SDCLOCK_PERIOD; sdramHandle.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE; sdramHandle.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_0;- LTDC: 2 MHz.
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_LTDC;
PeriphClkInitStruct.PLLSAI.PLLSAIN = 192; PeriphClkInitStruct.PLLSAI.PLLSAIR = 5; PeriphClkInitStruct.PLLSAIDivR = 2; HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct);While I'm getting data in norflash, LCD have prolems is flickering.
I know that LTDC will gennerate data to LCD automatically after SDRAM refresh, isn't it?
What is solution to hold data on LTDC while other device use bus data of SDRAM (16 bit data)?
Can you tell me solutions to fix that bug, please?
Thank you so much!
2019-03-17 08:50 PM
Dear @Manoj Chandran
Did you solve this problem ?
I'm facing the same problem with below information
Tearing effect in TFT LCD also occur.
I'm very appreciate if you help me to solve it
Thanks and best regards
2019-03-18 01:35 AM
2019-03-18 02:02 AM
So what rate are you clocking the display?
==> 33MHz.
How wide is you SDRAM interface?
==> 32 bit
For more information, I already config Pixel clock and timings configuration as TFT LCD specification but it does not work.
2019-03-18 02:13 AM
Exact same display, I'm assuming.
Under what circumstances is display tearing? All the time, when image static, when you are accessing SDRAM concurrently? What are caching and MPU settings for memory regions?
2019-03-18 02:18 AM
Display tearing occur when I display a background (800x400) image with rich gradient.