2017-10-20 04:17 AM
Hi, I have downloaded stm32cubef4 for the nucleo-64 board (stm32f401). The directory seems to have the correct structure. No icon has appeared on the desktop or in the launch menu (win10) to start the program. Anyone know how to get it started? Thanks
2017-10-20 04:32 AM
Hello,
Delete the package and try again the correct download of the firmware package
from STMicroelectronics official site:
.Or download the package directly from STM32CubeMx:
MENU > Help > Install New Libraries
Select libraries that you need
Force download with button “Install Now�.
Best Regards
Imen
2017-10-20 06:11 AM
2017-10-20 06:36 AM
Hi, It wont let me download the package again
2017-10-20 08:59 AM
Hi, I have re downloaded the package and extracted the files succesfully (I think). Now what do I do to install it?
2017-10-20 09:17 AM
I downloaded from the st site. I downloaded the AC6 toolchain and installed it.
2017-10-20 10:00 AM
It is an archive of files, what you need to do is down load and install the CUBEMX package, and use it to install the .ZIP
http://www.st.com/en/development-tools/stm32cubemx.html
Now if you just want to build things from AC6, you're going to need to navigate the package you unpacked, and open the PROJECTS within in it from your tool chain. The archive contains the HAL libraries, and an array of examples for assorted boards and peripherals.
2017-10-20 10:23 AM
thank you Clive, I shall try that