cancel
Showing results for 
Search instead for 
Did you mean: 

Need help for Keil project for STM32F Nucleo-32 with STM libraries

Randy Nelson
Associate III
Posted on October 20, 2017 at 20:49

Am trying to generate a Keil Uvision project to evaluate (and possibly expand) for the STM32F303 Nucleo-32. I prefer not to use the STM32Cube or HAL interface and remain at a lower level. I have the STM standard Peripheral library but I'm unable to start a Keil project using it. Can anyone offer any guidance? Thanks...

1 REPLY 1
Posted on October 22, 2017 at 15:10

>>

I'm unable to start a Keil project using it.

Not using F3's, but why would that be?

Can you take an SPL Template project, clone that and tweak the target settings and command line defines?

If it doesn't have an F303 pick something close and change the memory sizes, and startup.s to accommodate the differences.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..