2017-11-21 10:24 AM
In Cortex M3, what is the order in which the register are pushed into the stack?
Which of the following orders are correct (if any)?
First Order:
PC
PSRx
R3
R2
R1
R0
R12
Link Register
Second Order:
PC
PSRx
R0
R1
R2
R3
R12
Link Register
Please Guide? Thanks in advance?
#cortex-m3 #stm32f103rb #exception #arm2017-11-21 10:34 AM
JW
2017-11-21 12:03 PM
2017-11-21 12:12 PM
void hard_fault_handler_c(unsigned int * hardfault_args, unsigned int r4, unsigned int r5, unsigned int r6)
{ printf ('\n[Hard Fault]\n'); // After Joseph Yiuprintf ('r0 = %08X, r1 = %08X, r2 = %08X, r3 = %08X\n',
hardfault_args[0], hardfault_args[1], hardfault_args[2], hardfault_args[3]); printf ('r4 = %08X, r5 = %08X, r6 = %08X, sp = %08X\n', r4, r5, r6, (unsigned int)&hardfault_args[8]); printf ('r12= %08X, lr = %08X, pc = %08X, psr= %08X\n', hardfault_args[4], hardfault_args[5], hardfault_args[6], hardfault_args[7]);printf ('bfar=%08X, cfsr=%08X, hfsr=%08X, dfsr=%08X, afsr=%08X\n',
*((volatile unsigned int *)(0xE000ED38)), *((volatile unsigned int *)(0xE000ED28)), *((volatile unsigned int *)(0xE000ED2C)), *((volatile unsigned int *)(0xE000ED30)), *((volatile unsigned int *)(0xE000ED3C)) );while(1);
}2017-11-21 12:13 PM