cancel
Showing results for 
Search instead for 
Did you mean: 

How to decrease the VL53L0X FOV?

Diego Barile
Associate
Posted on October 23, 2017 at 16:13

Hello.

Does anybody knows if is possible to decrease the VL53L0X FOV putting in front of It a short piece of plastic (dark?) pipe?

Could it works enough fine or the cross-talk will become unacceptable?

Any other options to decrease the detecting FOV?

Thanks in advance.

#vl53l0x-fov-decrease-narrow-angle
1 REPLY 1
John E KVAM
ST Employee
Posted on January 02, 2018 at 19:48

Unfortunately there is no way to reduce the FOV. One would have to put a lens over the receive side of the chip and that would be very expensive.

I did have one customer who used two sensors side by side and at slightly different angles. As the target moved from right to left, the one sensor would get a range, when the second sensor also got a range, the machine 'knew' the leading edge of the target was in the small over-lapping FoV.

But this wouldn't work for everyone.

- john


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question. It helps the next guy.