2017-11-04 12:14 PM
MCU: STM32F777II, running at 64MHz
Source UART: UART4 (DMA Stream configured on both RX,TX), Baud Rate: 9600
Destination UART: UART8
(DMA Stream configured only for RX), Baud Rate: 9600
I need to bypass data coming on UART4 to UART8 not using any DMA channel, so I wrote the following code:
unsigned char strbfr[4] = '';
while(1)
{ // Block read (GPS connected) while(HAL_UART_Receive(&UART_INT, strbfr, 1, HAL_MAX_DELAY) != HAL_OK); // Write data on destination UART while(HAL_UART_Transmit(&UART_BT, strbfr, 1, 100) != HAL_OK); while (HAL_UART_GetState(&UART_BT) != HAL_UART_STATE_READY); }I see that that when the application runs, only few characters from the source i.e. the GPS device (which produces data continuously at 500ms burst rate) gets printed on the destination UART and then it stops sending. Is there any issue with this code? Is it because both source and destination are running at same baud rate? I observe that if i increase the baud rate of destination
UART8 to greater than 9600, the code runs fine, however I want to run UART8 at 9600 only due to peripheral constraints.
#stm32f72017-11-04 12:29 PM
2017-11-04 01:36 PM
Can you please explain this in detail Clive maybe via code example, how to do this
concurrently?
2017-11-04 01:50 PM
I use FIFO (Ring) Buffers that I fill using the USART RXNE interrupts, the foreground loop then checks the USART TXE state and if a character is in available in the FIFO, if there is I output the character. The loop does not block as it monitors two USART.
The FIFOs don't need to be too deep, but provides some elasticity to manage the ebb-and-flow of data and slight differences in framing or inter-symbol gaps.
It can also be done without interrupts, there the loop would test of the USART RXNE, ie
while(1) // USART Forwarder USART1<->USART2
{
if (USART1->SR & RXNE) FifoBufferStore(Fifo1, USART1->DR);
if (USART2->SR & RXNE) FifoBufferStore(Fifo2, USART2->DR);
if ((USART1->SR & TXE) && (!FifoBufferEmpty(Fifo2)) USART1->DR = FifoBufferLoad(Fifo2);
if ((USART2->SR & TXE) && (!FifoBufferEmpty(Fifo1)) USART2->DR = FifoBufferLoad(Fifo1);
// Check overrun/framing errors, etc
}
2017-11-04 05:16 PM
Thanks for the reply clive, is it possible if you can share some codes for
interrupt based logic for the same?
2017-11-05 04:40 AM
Hello,
If I understand you want a code example that acts as a bridge between 2 UART? Like a Serial Pass Trough.
You can take inspiration from my project below which works on a STM32F723 Discovery and which allows to transmit each character received from one UART to another bidirectionally (take a look to wiki page for more informations)
https://github.com/rreicher/32F723EDiscovery_SerialBridge
This should be easy to works on an STM32F777.
The repository contains the Cube configuration file.Bets regards
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.