cancel
Showing results for 
Search instead for 
Did you mean: 

Can't connect Nucleo 32 to USB

Peter Young
Associate
Posted on November 02, 2017 at 04:44

I’ve been through all the documentation and I’m getting very frustrated with this eval kit - it really shouldn’t be this difficult!

Installed latest USB drivers, however the device is still not showing up under device manager->USB devices and obviously ST-Link says “no St-Link detected�?. I have made sure I followed the power supply sequence for USB-enumeration to succeed. Also tried several different USB cables & USB ports.

Running Win

FWIW I have a STM32F469NIH6 DISCO kit that works with ST-link and the drivers mentioned above.

Any help would be much appreciated.

1 REPLY 1
S.Ma
Principal
Posted on November 02, 2017 at 10:08

Is the used USB port the ST Link one?