cancel
Showing results for 
Search instead for 
Did you mean: 

cubemx

Robert Goszty?a
Associate
Posted on November 09, 2017 at 19:46

Hi

I'm using newest possible CubeMX version. Trying to generate project for some environment, in this case SW4STM32 (however tool does not matter) and got this window. Code is generated, only project cannot be done. Java installed is 9.0.1.

0690X0000060PCJQA2.png

Checking Java output got something like this:

2017-11-09 19:40:01,978 [INFO] ProjectBuilder:1369 - Project Generator version: 2.0

2017-11-09 19:40:01,988 [INFO] ConfigFileManager:343 - The Die is : DIE410

2017-11-09 19:40:02,013 [INFO] ToolchainGenerator:103 - [Project Generator] Problem in the project generation

java.lang.ClassCastException: parsers.SysWbParser cannot be cast to parsers.FromScratchParser

at convertor.Convertor.convert(Convertor.java:546)

at convertor.Convertor.generate(Convertor.java:349)

at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.generate(ToolchainGenerator.java:99)

at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createToolChainFolders(ProjectBuilder.java:1408)

at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:508)

at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:41)

2017-11-09 19:40:02,021 [INFO] ProjectBuilder:1424 - Time for Generating toolchain IDE Files: 44mS.

2017-11-09 19:40:02,022 [ERROR] ProjectBuilder:1430 - Error in Project Generation

2017-11-09 19:40:02,022 [ERROR] ProjectBuilder:524 - Error in Project Generation

Any help is welcome.

BR, Robert

0 REPLIES 0