cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DH or LIS331H @ 4.2V ?

Vlado Velicky
Associate
Posted on November 17, 2017 at 14:02

Hello,

I'm trying to design device with all components powered by li-po battery to minimize the power losses, cost and SIZE.

I'd like to avoid voltage regulator, level shifters etc.

This sensors should be powered up to 3.6 V, but the maximum ratings are high above @ 4.8V.

Would it be possible to power LIS3DH with voltage up to 4.2 V?

Is anybody using these sensors @ 4.2 V ?

Thank you in advance.

0 REPLIES 0