2017-11-27 07:08 PM
Dear there,
I'm using the Nucleo STM32L031K6 EVK as a 12MHZ SPI slave in my application. Now I found it takes about 60ms from VDD ready to finishing excetution of below code snippet so the SPI slave misses some cmd of SPI master. How can I reduce the boot time to below 20ms(lesser is better)? Thank you very much.
HAL_Init();
/* Configure the system clock to 32 MHz */
SystemClock32m_Config(); MX_GPIO_Init();//============================
void SystemClock32m_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInit;
/**Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_4;
RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler(__FILE__, __LINE__);
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler(__FILE__, __LINE__);
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_I2C1;
PeriphClkInit.I2c1ClockSelection = RCC_I2C1CLKSOURCE_PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler(__FILE__, __LINE__);
}
/**Configure the Systick interrupt time
*/
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/**Configure the Systick
*/
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
#stm32 #spi #boot-time
2017-11-29 02:07 AM
Hi There,
I have new finding today. Actually, on the entry of the main() it already takes about 60ms.
So what happen before that? I went through the Reset_Handler and found it just call SystemInit before branching into main( ). And the SystemInit looks simple. So how does the 60mS come from? Any idea is appreciated.
2018-02-09 02:39 AM
Hi There,
I have the same problem with stm32L452. From reset to main it takes more than 4ms which is too long for my apllication. Have you found a solution for the long boot time ?
2018-02-09 09:44 AM
2018-02-09 11:00 AM
'
How can I reduce the boot time to below 20ms(lesser is better)?
'
not sure how you measured it but it is entirely possible that the actual time is considerably shorter / longer than what you thought it was.
with that said, a few things will help you speed up the process:
1) use an external oscillator - hopefully with a quick start-up time.
2) disable PLL.
3) roll your own configuration code so you don't incur the library related bloat. 60ms for a 32-bit chip is like enternity.
4) the most effective: start your chip first before anything else.
...
2018-02-09 05:02 PM
If you have a low impedance power supply,
the 3V rise time would be sharper,
then your reset would be quicker.
but you may only gain 10-20mS.