2017-11-30 04:54 AM
Hi,
I'm working with a STM32L053R8 and I want to use some ADC pins. I have a doubt about the input voltage range.
Does the ADC have an independent power supply?
Which is the input voltage range of the ADC?
For example:
Let's suppose that I am supplying the STM with 3.3 V, and I am using 12 bits from the ADC.
That means that...?
- The input voltage range goes from 0V to 3.3V?
- The step-quantization is 3.3/(2^12-1)?
Thanks!
🙂
#hal #adc #stm32 #stm32l0 #voltage-reference #voltage-range #adc-supply2017-11-30 06:07 AM
Does the ADC have an independent power supply?
Together with other analog circuits (e.g. DAC), VDDA/VSSA, which is by datasheet required to be connected to the 'digital' VDD/VSS (often through a small inductor in role of a filter).
Which is the input voltage range of the ADC?
VREF- to VREF+. On small packages, VREF- is internally connected to VSSA and VREF+ to VDDA.
Let's suppose that I am supplying the STM with 3.3 V, and I am using 12 bits from the ADC.
That means that...?
- The input voltage range goes from 0V to 3.3V?
- The step-quantization is 3.3/(2^12-1)?
Yes, unless - as said above - you have separate VREF different from VDDA.
JW