2017-11-30 06:24 PM
I'm currently programming a bootloader for my project. I work on a STM8AF board and I have a problem with the write memory command.
I follow each instruction in the UM0560 user manual. My problem appears at the end of the sequence, I never receive the last ACK or NACK.
Example (I use the UART peripheral) :
-I send my first byte 0x31 and 0xCE his complement. -The device answer with ACK (0x79).-I send the address 0x00 00 80 00 and the checksum 0x80.-The device answer with ACK.-I send the number of bytes, the data 0x01 0x53 and the checksum 0x52And here the device stop answering hereI check in ST Visual Programmer, the ROP byte is disable and the data is never written.
Attached, my trace in Hercules and the sequence in UM0560 user manual.
Thanks,
Alexandre
#stm8a #uart #bootloader #write-memory2017-12-01 02:13 AM
Hello Alexandre ,
i am moving this post on STM8 Side 😉
Best regards
Erwan