2017-12-08 01:11 AM
It is mentioned that muRata has a collaboration with you on bringing sigfox to their Type ABZ lora module. However I can only find news about it, not actually something concrete on how and what. Could you please link me to more info.
Heres the news article.
#murata-cmwx1zzabz #sigfox #lora2017-12-08 09:12 AM
I guess there will be an announcement when it's released?
Meanwhile, have you tried contacting muRata?
2017-12-08 09:57 AM
2017-12-11 12:26 AM
Thanks all for your reply.
I did first contact muRata. But I haven't heard from them yet. And no info on their website.
2017-12-11 07:05 AM
2017-12-27 05:55 AM
Hi All,
for your information, the
from company is a dual-mode LoRa-SigFox certified module for European countries. It is in MP since mid 2015. This module uses SX1272 transceiver from Semtech and STM32 microcontroler from ST.2017-12-29 06:55 AM
Thanks for that, but the details on that page (and the Wiki) are pretty sketchy - is there a full datasheet and/or user manual available?
Which STM32 does it use?
Is the stack open-source - like the muRata module ?
2017-12-29 07:25 AM
Hi Andrew,
At the end of the Wiki page, you have all the documents :
Module Datasheet :
http://wiki.nemeus.fr/images/4/4f/MM002-xx-EU_datasheet_v1.1.pdf
List of AT commands :
http://wiki.nemeus.fr/index.php?title=MM002-xx-EU_AT_Commands
This module uses STM32L151 version.
The stack is a full development from NEMEUS (compliant with SigFox and LoRa WAN Class 1.0.2) and the module (HW & SW parts) has been certified against SigFox, Objenious and Orange networks. This one is also used by some customers with other networks like Proximus, KPN, SwissCom, etc ...
NEMEUS provides a full certified module ready to use with operators (including IDs and Keys) and not only HW part as some other module providers.
Under some agreement, it is possible for customer to embed its applicative software into the module.
Regards
2017-12-29 10:24 AM
Oh yes - I see them now!
2018-02-23 02:12 AM
Looks like it's finally arrived:
http://blog.st.com/x-cube-sfox-firmware-sigfox/
http://www.st.com/x-cube-sfox?icmp=tt6591_gl_lnkon_feb2018
, launching today, is the first STM32Cube expansion package offering a SigfoxTM stack compatible with the Murata CMWX1ZZABZ-xxx modules.http://www.st.com/en/embedded-software/x-cube-sfox.html?icmp=tt6591_gl_lnkon_feb2018