cancel
Showing results for 
Search instead for 
Did you mean: 

SPC560B64L7 FlexCAN bootloader

Poon Jon
Associate
Posted on December 18, 2017 at 04:05

Hi, I'm currently using a SPC560B64L7 and I wish to go into bootloader via FlexCAN without connecting pin PA[8] and PA[9], is this possible to do so? Best if I could do all this in my application code.

1 REPLY 1
Erwan YVIN
ST Employee
Posted on December 19, 2017 at 10:08

Hello Poon Jon ,

on SPC56, to use the bootloader via FlexCan, you should enable ABS and FAB.

FAB and ABS pins is implemented on SPC56 family

on SPC57,SPC58 ,the internal signals, which were originally driven by those pins, is tied to ´0´.

I think that you should create your own bootloader.

Anyway , I will check with experts.

             Best regards

                                       Erwan