2017-12-21 04:38 AM
Hello,
Having a problem to startup the STM32L4 MCU. After powering the board it seems like the controller does not start or get stuck. Running with a debugger works fine but when removing the debugger connection and power cycle the board, the controller does not run. I also tested to add an external watchdog and the controller started and behaved as expected. So I started to think that the reset (NRST) pin had to do with the problem. I removed the external watchdog and power cycled the board then I manually reset the MCU by shortly connected the NRST to ground. The MCU started to run as expected.
I would prefer to run without an external watchdog and without a manual reset. I am asking for help to understand why this is happening and how to solve the problem.
Solved! Go to Solution.
2017-12-21 04:47 AM
2017-12-21 04:47 AM
2017-12-22 12:12 AM
Do you have a 100nF capacitor connected from Reset to Vss?
Is your power supply startup ramp monotonic?
2017-12-22 04:26 AM
Hi,
The BOOT0 was not connected so I connected BOOT0 to GND and now the controller works as expected.
Regarding John F’s comment, there is no capacitor between Reset and Vss. It is a capacitor 100nF between Reset and GND. The startup ramp looks fine.
Thank you both for all help!