cancel
Showing results for 
Search instead for 
Did you mean: 

LIN sensor problem

jiang jun
Associate
Posted on December 27, 2017 at 04:15

I have a Pepper+Fuchs sensor which interface is LIN(attachements are datasheet & user manual ). I need to test the sensor by computer so I purchased RS232 to LIN converter. I send 

handshake command on computer to the converter and it respone telegram correctly. The telegram format of converter is as below:

0690X00000609IsQAI.png

While 

telegram format of Pepper+Fuchs sensor is as below. When i send telegram following below to the sensor, there is no respone at all. Due to the 2 type telegram format is different , i don't know where is the problem. Is there anyone can help me?

0690X00000609IwQAI.png

#232-lin-converter
1 REPLY 1
Erwan YVIN
ST Employee
Posted on January 08, 2018 at 10:32

Hello ,

this component is using 'Interface Interface type Physical LIN interface Transfer rate 19.2 kBit/s (8N1) Cycle time 100 ms'

i do not think that it is a ST device.

i recommend you to contact Pepper Fuchs community website

               Best regards

                     Erwan