cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-SPIN3202 is Not included in the ST Motor Profiler

yanjae huh
Associate
Posted on December 28, 2017 at 01:58

Good morning!

I bought Steval-Spin3202, but there is no choice in the SDK for this board.

Is this board not supported by the current version of the SDK?

What are some ways I can try this board?

2 REPLIES 2
Enrico Poli
ST Employee
Posted on January 04, 2018 at 14:14

Hi,

the board is not included into the list of the MC workbenchboards.

However you can set the parameter in order to obtain a compatible project (attached)

________________

Attachments :

SDK43x-STEVAL-SPIN3202-BullRunning.stmcx.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyBP&d=%2Fa%2F0X0000000b4m%2F_O3am0cwXNnLk.yhMQg6tlUsTnGpSLoY0dTBA05sOkM&asPdf=false
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards