cancel
Showing results for 
Search instead for 
Did you mean: 

FreeRTOS and CAN driver for STM32F767 Nucleo board

yalamanda dosakayala
Associate II
Posted on March 21, 2018 at 07:37

Hi STM community,

I have STM32F767 nucleo board, As per my project requirements I need FreeRTOS and CAN driver for this Nucleo board.

I have downloaded latest SDK1.11 , but I didn't found any such example projects.

Can any help me , is there any sample projects related to this board.

or if no sample project , Can anyone guide me how do I start implementing the FreeRTOS and CAN driver.

#nucleo-stm #can #stm32-f7 #freertos
4 REPLIES 4
Richard Lowe
Senior III
Posted on March 21, 2018 at 08:27

When using an RTOS you need to think about the actions (inputs, outputs) that are taking place. CAN does a couple of things, receives and transmits. Therefore, you could specify 2 tasks, 1 for RX and the other for TX duties.

/**
 * @brief All reception of CAN messages are processed
 *
 * Process is ran when the CAN RX interrupt passes the CAN_RX_ISR_FLAG. This
 * represents at least a single packet on the FIFO. All mailboxes are processed
 * and queued to the proper handler.
 *
 * @param argument task arguments - none needed
 */
void can_rx_process( void const * argument )
{
 osEvent evt;
 uint8_t data[8];
 CAN_RxHeaderTypeDef rx_msg;
 HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING | CAN_IT_ERROR );
 for( ;; )
 {
 evt = osSignalWait( CAN_RX_ISR_FLAG | CAN_ERR_ISR_FLAG, WDT_MAX_WAIT_TIME );
 if( evt.value.signals & CAN_RX_ISR_FLAG )
....�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

This is a CAN RX task that waits for the interrupt coming from messages pending.

/**
 * @brief Transmission of all CAN messages originate from this task
 *
 * @param argument
 */
void can_tx_process( void const * argument )
{
 osEvent evt;
 CAN_TxHeaderTypeDef tx_msg;
 uint8_t msg_data[8];
 uint32_t mailbox;
 osTimerStart( heartbeat_timer, CAN_HEARTBEAT_DELAY );
 for( ;; )
 {
 evt = osMessageGet( can_tx_handle, WDT_MAX_WAIT_TIME );
 if( evt.status == osEventMessage )
 {
 message_t *msg = (message_t*) evt.value.p;
....�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

This is a task that waits for another task to send a `message_t` to it.

Yes there are some extras in there you don't need but the principles are the same. Both tasks wait for some work to perform. The RX task waits for the interrupt of messages pending, the TX task waits for another task to send it some message to send.

Posted on March 21, 2018 at 10:56

Hi

Lowe.Richard

, thank you for reply, But I need code for the CAN driver for STM32F767 Nucleo board.

Is there any sample project for the CAN driver for Nucleo board.

Please share me the link

Posted on March 21, 2018 at 18:53

There really isn't any 'driver' for CAN on the STM32. It is a hardware peripheral, so it's all about configuring the peripheral to your purposes. Any of the CAN demos in the STM32 repos demonstrate this. If the STM32F767 has CAN then the `<STM32CubeInstallDir>/Repository/STM32Cube_FW_F7_V1.11.0/Projects/STM32F769I_EVAL/Examples/CAN/CAN_Networking` for example.

Posted on March 21, 2018 at 20:45

You're likely to have to take responsibility for your own project execution and porting from close approximations to your hardware. The examples for the EVAL series boards tend to be richer than the NUCLEO as they have many hardware interfaces already added/implemented. If you really need zero effort implementations consider buying an EVAL board with the feature set required.

ST also maintains list of contractors and consultants if you need professional guidance or direction. If you represent a large commercial client FAE resources may also be available.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..