cancel
Showing results for 
Search instead for 
Did you mean: 

run motor without the use of st motor control workbench

Low Yik Seong
Associate III
Posted on January 08, 2018 at 16:08

Hi, I am trying to modify the the code which is compiled from st motor control workbench. So far i have successfully run using st motor control workbench. May I ask is it possible to modify the code so that it does not need to run through the st motor control workbench which include adjusting the speed of motor just by varying the potential-meter on motor driver. If it is possible, which document do I need to refer to? Thanks

1 REPLY 1
Erwan YVIN
ST Employee
Posted on January 09, 2018 at 10:12

Hello , 

I am not responsible of ST motor control library.

I am contacting the development team about this request.

   Best regards

         Erwan