cancel
Showing results for 
Search instead for 
Did you mean: 

LM358: Circuit verification

jom sabu
Associate
Posted on January 12, 2018 at 12:26

Hello Sir,

We have used opamp ic LM358 in our audio project, which used for amplification of signal from mic to adc of microcontroller.

Could you please verify the attached circuit, let me know if you have any comments.

Regards

Jom

1 REPLY 1
Pierre SENNEQUIER
ST Employee
Posted on January 25, 2018 at 10:54

Hi Sir,

The cutoff frequencies are too high for audio signal (10nF and 1kOhm => 15.9kHz and 1.5nF and 330 Ohm => 322kHz).

If you want to keep the gain unchanged, you should increase the 10nF and 1.5nF capacitors to respectively at least 10uF and 22uF.

  Best Regards,

P

In order to give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.