cancel
Showing results for 
Search instead for 
Did you mean: 

ST25R3911DiscoComm.dll Need sample code usage

Ivan Smolin
Associate II
Posted on January 16, 2018 at 18:10

Or source code of 'ST25R3911B Discovery.exe' (1.1.16.0)

Yes, I really want some of it because ST25SDK is not applicable for me.

(See my previous question for details)

But it is better to just give me some source code - I waiting too long!

1 ACCEPTED SOLUTION

Accepted Solutions
Ulysses HERNIOSUS
ST Employee
Posted on January 17, 2018 at 15:48

Hi Ivan,

If you look into the installation directory of ST25R3911B-DISCO GUI you will find: 

  • ST25R3911DiscoComm.dll 
  • ST25R3911DiscoComm.h : prototypes for all functions
  • ST25R3911DiscoComm.lib : lib to be used when the DLL should be used by C/C++
  • iso14443a_select_by_uid.py : Small Python example showing usage of the DLL for ISO14443A only - the second part of it may not so interesting for you - direct select without previous anitcollision is rarely used.

This should enable you to understand the basic usage of the DLL.

Regards, Ulrich

View solution in original post

2 REPLIES 2
Posted on January 16, 2018 at 18:14

Perhaps contact your local ST sales office and the FAE's working out of there.

https://community.st.com/0D50X00009XkWobSAF

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Ulysses HERNIOSUS
ST Employee
Posted on January 17, 2018 at 15:48

Hi Ivan,

If you look into the installation directory of ST25R3911B-DISCO GUI you will find: 

  • ST25R3911DiscoComm.dll 
  • ST25R3911DiscoComm.h : prototypes for all functions
  • ST25R3911DiscoComm.lib : lib to be used when the DLL should be used by C/C++
  • iso14443a_select_by_uid.py : Small Python example showing usage of the DLL for ISO14443A only - the second part of it may not so interesting for you - direct select without previous anitcollision is rarely used.

This should enable you to understand the basic usage of the DLL.

Regards, Ulrich