cancel
Showing results for 
Search instead for 
Did you mean: 

Can you confirm that the STM32F4 is pin-to-pin compatible with the STM32L4 please ?

HAMADI Gratien
Associate
Posted on January 16, 2018 at 11:00

http://www.st.com/en/microcontrollers/stm32l4-series.html?querycriteria=productId=SS1580

 

'

To simplify migration and give you all the flexibility you need, the STM32L4 is pin-to-pin compatible with the different STM32 series and opens the door to the full STM32 ecosystem.'

1 REPLY 1
Posted on January 16, 2018 at 11:53

This docs might be interesting:

http://www.st.com/content/ccc/resource/technical/document/application_note/group0/02/46/be/cf/31/75/4e/de/DM00263732/files/DM00263732.pdf/jcr:content/translations/en.DM00263732.pdf

 

'

STM32L4 Series / STM32L4+ Series as well as STM32F405/415 and STM32F407/417 lines

share a high level of

pin

compatibility.

Most peripherals share the same

pin

s.

The transition from STM32F405/415 and STM32F407/417 lines to STM32L4 Series /

STM32L4+ Series is simple since only a few

pin

s are different.'