cancel
Showing results for 
Search instead for 
Did you mean: 

PIN outs for HTS221

steve sagerian
Associate II
Posted on January 28, 2018 at 06:52

Is the pin out diagram on page 6 which is labeled ''bottom view'' actually a view from the top? 

VCC is in the upper left corner (pin 1).  The top side view shows the pin 1 ''dot'' also in the top left corner. 

and finally the mech drawing shows another bottom side view which contradicts the figure 2 drawing..

whats correct?

thanks

0690X00000609VlQAI.png0690X00000609W5QAI.png0690X00000609VqQAI.png
5 REPLIES 5
steve sagerian
Associate II
Posted on January 28, 2018 at 06:55

actually I see that the mech drawing is actually rotated so it matches the figure 2 drawing but the tops side pin 1 mark still seems incorrect.

Posted on January 29, 2018 at 10:24

All three picture are correct.

I have rotated the picture with pinout by 90 degrees so it should clear now.

0690X00000609X8QAI.png
Posted on January 29, 2018 at 14:37

Just to confirm this is the bottom view, for making a pcb model I would need to flip it along the vertical access so that the pin 1 is in the upper left corner?

Posted on January 29, 2018 at 14:41

vertical axis...access sheeee!

Posted on January 29, 2018 at 15:30

Yes, you are right.