2018-01-18 12:50 AM
Hello everyone,
I'm trying to make a device where the MCU (STM32L151) has to wake up periodically every 5 minutes and send a LoRa message. As such i want to put the device in a low power mode between messages. I read up on the datasheets and manuals on how to do this and decided to use the HAL. Now when i put the device to sleep it does not wake up anymore...
I would like to note that everything works perfectly when i use the 'normal' power mode (ie. not touching any power settings).
I want the device to wakeup from either:
In the code below you can see i use
HAL_PWR_EnterSLEEPMode. while the mcu enters the low power mode, it does not exit on the pin or RTC interrupt. I have also tried HAL_PWR_EnterSTOPMode() and HAL_PWR_EnterStandbyMode(), but the result stays the same.
while (1) {
//if device is open when battery is just inserted the device has to wait till case is closed if (caseprotector_get_state() >= closed_protected) { /* run the LoRa class A state machine*/ lora_fsm();if (lora_getDeviceState() == DEVICE_STATE_SLEEP) {
HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);}
}Code for initializing the interrupt pin (PC13):
void MX_GPIO_Init(void)
{GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE() ; __HAL_RCC_GPIOA_CLK_ENABLE() ;/*Configure GPIO pin Output Level */
/*Configure GPIO pin : PtPin */
GPIO_InitStruct.Pin = Security_Switch_Pin; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING; GPIO_InitStruct.Pull = GPIO_PULLDOWN; HAL_GPIO_Init(Security_Switch_GPIO_Port, &GPIO_InitStruct);/* EXTI interrupt init*/
HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0); HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);}
Initializing the RTC:
/*!
* @brief Configures the RTC timer * @note The timer is based on the RTC * @param none * @retval none */static void HW_RTC_SetConfig( void ){ RTC_TimeTypeDef RTC_TimeStruct; RTC_DateTypeDef RTC_DateStruct;RtcHandle.Instance = RTC;
RtcHandle.Init.HourFormat = RTC_HOURFORMAT_24;
RtcHandle.Init.AsynchPrediv = PREDIV_A; /* RTC_ASYNCH_PREDIV; */ RtcHandle.Init.SynchPrediv = PREDIV_S; /* RTC_SYNCH_PREDIV; */ RtcHandle.Init.OutPut = RTC_OUTPUT; RtcHandle.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH; RtcHandle.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;HAL_RTC_Init( &RtcHandle );
/*Monday 1st January 2016*/
RTC_DateStruct.Year = 16; RTC_DateStruct.Month = RTC_MONTH_JANUARY; RTC_DateStruct.Date = 1; RTC_DateStruct.WeekDay = RTC_WEEKDAY_MONDAY; HAL_RTC_SetDate(&RtcHandle , &RTC_DateStruct, RTC_FORMAT_BIN);/*at 0:0:0*/
RTC_TimeStruct.Hours = 0; RTC_TimeStruct.Minutes = 0;RTC_TimeStruct.Seconds = 0;
RTC_TimeStruct.TimeFormat = 0; RTC_TimeStruct.SubSeconds = 0; RTC_TimeStruct.StoreOperation = RTC_DAYLIGHTSAVING_NONE; RTC_TimeStruct.DayLightSaving = RTC_STOREOPERATION_RESET;HAL_RTC_SetTime(&RtcHandle , &RTC_TimeStruct, RTC_FORMAT_BIN);
/*Enable Direct Read of the calendar registers (not through Shadow) */
HAL_RTCEx_EnableBypassShadow(&RtcHandle);}Lastly i would like to add that i don't have a lot of experience with the ST MCU's.I hope someone can help me with this problem.
If you have further questions please ask them, i'll be happy to answer them!
Kind regards,
Jesse Bax,
Jr software developer
#rtc-wakeup #low-power-standby #stm32l1 #stm32-standby-wake-rtc2018-09-24 02:45 AM
Hey jesse
i'm working with STM32L072, so i'm not sure if it's exactly the same with your MCU.
i ha a lot of troubles getting the device to sleep, following code finally did the trick for me.
don't get irritated by the FreeRTOS stuff 😉 maybe this helps
cheers matt
/* Set RTC*/
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc,u16TimeToStop,RTC_WAKEUPCLOCK_CK_SPRE_16BITS;
/* suspend scheduler*/
vTaskSuspendAll();
/* disables irq, interrupts will still be able to wake up the system*/
__disable_irq();
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_RCC_WWDG_CLK_DISABLE();
HAL_PWREx_EnableUltraLowPower();
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON,PWR_STOPENTRY_WFI);
/* System sleeps here*/
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
/* on wake up, restore system clock*/
HAL_RCC_DeInit();
SystemClock_Config();
__HAL_RCC_WWDG_CLK_ENABLE();
/* check interrupts now*/
__enable_irq();
/* stop RTC */
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
RTC_LORAMAC = bTRUE;
/*resume scheduler*/
xTaskResumeAll();