2018-02-02 03:34 AM
Hi all,
I am trying to make a simple CAN test program to send 8 bytes data.
It seems like it is sending data (from the code point of view) but when I look with a scope. The TX line goes down for a few �S, then go back high and that's it. It seems like it doesn't transmit anything at all....
I got the interrupt with HAL_FDCAN_TxFifoEmptyCallback() called but also the HAL_FDCAN_ErrorCallback()...
This is the config:
static void MX_FDCAN1_Init(void)
{
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC; hfdcan1.Init.Mode = FDCAN_MODE_NORMAL; hfdcan1.Init.AutoRetransmission = DISABLE; hfdcan1.Init.TransmitPause = DISABLE; hfdcan1.Init.NominalPrescaler = 16; hfdcan1.Init.NominalSyncJumpWidth = 9; hfdcan1.Init.NominalTimeSeg1 = 4; hfdcan1.Init.NominalTimeSeg2 = 3; hfdcan1.Init.DataPrescaler = 4; hfdcan1.Init.DataSyncJumpWidth = 9; hfdcan1.Init.DataTimeSeg1 = 4; hfdcan1.Init.DataTimeSeg2 = 3; hfdcan1.Init.MessageRAMOffset = 0; hfdcan1.Init.StdFiltersNbr = 0; hfdcan1.Init.ExtFiltersNbr = 0; hfdcan1.Init.RxFifo0ElmtsNbr = 8; hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8; hfdcan1.Init.RxFifo1ElmtsNbr = 0; hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8; hfdcan1.Init.RxBuffersNbr = 0; hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8; hfdcan1.Init.TxEventsNbr = 0; hfdcan1.Init.TxBuffersNbr = 0; hfdcan1.Init.TxFifoQueueElmtsNbr = 4; hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION; hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8; hfdcan1.msgRam.StandardFilterSA = 0; hfdcan1.msgRam.ExtendedFilterSA = 0; hfdcan1.msgRam.RxFIFO0SA = 0; hfdcan1.msgRam.RxFIFO1SA = 0; hfdcan1.msgRam.RxBufferSA = 0; hfdcan1.msgRam.TxEventFIFOSA = 0; hfdcan1.msgRam.TxBufferSA = 0; hfdcan1.msgRam.TxFIFOQSA = 0; hfdcan1.msgRam.TTMemorySA = 0; hfdcan1.msgRam.EndAddress = 0; hfdcan1.ErrorCode = 0; if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
then the code :
HAL_FDCAN_ActivateNotification(&hfdcan1, 0xFFFFFFFF, 0xFFFFFFFF);
/* Start the FDCAN module */
if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK) { Error_Handler(); } /* Prepare Tx Header */ TxHeader.Identifier = 0x1; TxHeader.IdType = FDCAN_STANDARD_ID; TxHeader.TxFrameType = FDCAN_DATA_FRAME; TxHeader.DataLength = FDCAN_DLC_BYTES_8; TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE; TxHeader.BitRateSwitch = FDCAN_BRS_OFF; TxHeader.FDFormat = FDCAN_CLASSIC_CAN; TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS; TxHeader.MessageMarker = 1; /* USER CODE END 2 *//* Infinite loop */
/* USER CODE BEGIN WHILE */ while (1) {/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
//if (HAL_FDCAN_AddMessageToTxBuffer(&hfdcan1, &TxHeader, TxData, FDCAN_TX_BUFFER0) != HAL_OK) if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, TxData) != HAL_OK) { /* Transmission request Error */ Error_Handler(); } //if (HAL_FDCAN_EnableTxBufferRequest(&hfdcan1,FDCAN_TX_BUFFER0) != HAL_OK) { /* Transmission request Error */ // Error_Handler(); } HAL_FDCAN_ActivateNotification(&hfdcan1, 0xFFFFFFFF, 0); HAL_Delay(10); }#fdcan-stm32h7Solved! Go to Solution.
2018-02-02 07:01 AM
It is fixed now and working. The issue was the 5V not being properly connected on the MCP2542 click...
2018-02-02 03:37 AM
Why the source code formatting thing is not working ??
2018-02-02 03:51 AM
The error function is called with Protocol Error in Arbitration Phase.
Any idea why this would happen ?
2018-02-02 04:06 AM
2018-02-02 05:17 AM
I have a MCP2542 click connected to my nucleo and muxtrace to receive the packet.
But nothing. The fact that I got the interrupt error means that there must be something wrong with my can parameters.
2018-02-02 05:23 AM
I am using the demo code in
STM32Cube_FW_H7_V1.2.0\Projects\STM32H743I_EVAL\Examples\FDCAN\FDCAN_Classic_Frame_Networking
But I have the same issue, it doesn't send and I got the same error...
2018-02-02 07:01 AM
It is fixed now and working. The issue was the 5V not being properly connected on the MCP2542 click...