cancel
Showing results for 
Search instead for 
Did you mean: 

Problem in file system update using UART in SPWF01S

Jitendra NVS
Associate II
Posted on March 12, 2018 at 15:11

In SPWF01S wifi module, could perform File system update using AT+S.HTTPDFSUPDATE over the air with the help of Apache web server successfully (from Lab6 of Wi-Fi Training - Hands On  manual). 

But the same is giving problem using UART

(from Lab6 of 

Wi-Fi Training - Hands On  manual) 

after the below commands:

• AT+S. HTTPDFSWRITE=357957

• In Tera Term: File – Send File...

Not  prompting  to issue a reset command in order to complete the file system update, but hanging in the mid(PFA below). Please help me in solving this issue.

Thanks & Regards

Jitendra 

0 REPLIES 0