2018-02-14 10:30 PM
What are the non maskable interrupt I/Os are in STM32L431VCT6?. We plan to use External watchdog for our critical application.Output of WDT going to connected with NMI of STM32l431vct6.
2018-02-15 05:15 AM
The Reference Manual doesn't suggest such functionality
The internal watch dog does a Reset, that is 'non-maskable', use the NRESET pin to achieve the same.
2018-02-15 11:38 PM
Hi,
In case i use external watchdog timer, it has separate output for Watchdog reset and nReset. Where i have connect WDT output to controller's I/O?
2018-02-16 12:09 AM
You'll have to pick a GPIO and configure in EXTI functionality, but it will be maskable.
EXTI0 would have highest priority, pick one of PA0, PB0, PC0, etc.
2018-02-19 10:13 PM
Hi ,
I plan to use ESD diode on UART I/Os.My controller will run by 3.3v Source.If i choose ESD diode corresponding to my voltage levels, Clamping voltage is around 18v (8/20us). Will I/O support this volatge clamp for small duration?
2018-02-20 09:02 PM
Hi ,
I plan to use ESD diode on UART I/Os.My controller will run by 3.3v Source.If i choose ESD diode corresponding to my voltage levels, Clamping voltage is around 18v (8/20us). Will I/O support this volatge clamp for small duration?
2018-02-20 09:07 PM