2018-05-07 12:09 AM
I want to implement a low pass filter with cutoff frequency 50 kHz. How do I go about? I have gone through the example. But its not very clear.
2018-05-07 02:02 AM
Which example? What is not clear in it?
JW
2018-05-07 02:39 AM
Hi the example is arm_fir_example which is there in the following path:
C:\Keil_v5\ARM\CMSIS\DSP_Lib\Examples\arm_fir_example.
In this example they have done the following:
The input signal is a sum of two sine waves: 1 kHz and 15 kHz.
* This is processed by an FIR lowpass filter with cutoff frequency 6 kHz. * The lowpass filter eliminates the 15 kHz signal leaving only the 1 kHz sine wave at the output.The thing that is not clear is regarding the FIR coefficients generated.
They are using fir1() MATLAB function.
** fir1(28, 6/24) ,then storing the generated coefficients in the following buffer:const float32_t firCoeffs32[NUM_TAPS] = {
-0.0018225230f, -0.0015879294f, +0.0000000000f, +0.0036977508f, +0.0080754303f, +0.0085302217f, -0.0000000000f, -0.0173976984f, -0.0341458607f, -0.0333591565f, +0.0000000000f, +0.0676308395f, +0.1522061835f, +0.2229246956f, +0.2504960933f, +0.2229246956f, +0.1522061835f, +0.0676308395f, +0.0000000000f, -0.0333591565f, -0.0341458607f, -0.0173976984f, -0.0000000000f, +0.0085302217f, +0.0080754303f, +0.0036977508f, +0.0000000000f, -0.0015879294f, -0.0018225230f};However, if my input signal is different each time, how will i generate the FIR filter coefficients.
2018-05-07 05:13 AM
However, if my input signal is different each time, how will i generate the FIR filter coefficients.
Not sure if you understand the topic. Of course the input data will change continuously, that's what it's about.
You change filter coefficients if you want different parameters, like another cutoff frequency.
Hi the example is arm_fir_example which is there in the following path:
C:\Keil_v5\ARM\CMSIS\DSP_Lib\Examples\arm_fir_example.
This is an example from ARM, and describes the same. It is not a FIR/IIR filter tutorial.