cancel
Showing results for 
Search instead for 
Did you mean: 

The LIS3DH crash test reads an abnormal acceleration value

? ?_3
Associate II
Posted on April 10, 2018 at 04:14

     When I was doing impact testing, using the 16g range, with my device gently knock on the desktop, the acceleration values read have acceleration values of more than 10g, a bit unbelievable, acceleration reading and conversion are in accordance with In the manual, there should be no problem. When the plane is laid flat, the X and Y axes tend to be 0, and the z axis is about 1G. What causes this?

0690X00000604NOQAY.jpg
1 REPLY 1
Miroslav BATEK
ST Employee
Posted on April 10, 2018 at 10:40

What ODR do you use?

If high ODR is used (for example 400Hz) than you are able to capture the acceleration peaks which can be quite high (easily above 10g). The knock generates short impact with high g value, it is normal.