cancel
Showing results for 
Search instead for 
Did you mean: 

ST Visual Develop crashes when starting Tools -> Programmer

Thomas Miehle
Associate
Posted on March 16, 2018 at 07:23

I have been using ST Visual Develop with the STM8 Cosmic Compiler on a Virtual PC with Win10 for months.

Now I want to use it on my normal PC (also Win 10 64 bit  Version 1709), CosmicCompiler is working but I cannot program the code on the target (see picture), this  happens a soon as I open in the menu Tools->Programmer.

I installed the ST-Link utility and the ST Visual PÃœrogrammer, both can be started. The ST-Link V2 is correctly shown in the Device Manager of Windows.

I re-installed ST Visual Develop but this doesn't help.

Any ideas what is going wrong?
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on April 03, 2018 at 14:05

Hello,

Yes, issue already known.

See this post for a workaround :

https://community.st.com/0D50X00009XkWxBSAV

View solution in original post

6 REPLIES 6
raivo
Associate II
Posted on March 30, 2018 at 20:14

Same here...

0690X0000060ALIQA2.png0690X0000060ALJQA2.png

After selecting Tools->Programmer, I get:

0690X0000060ALNQA2.png
Posted on April 03, 2018 at 14:05

Hello,

Yes, issue already known.

See this post for a workaround :

https://community.st.com/0D50X00009XkWxBSAV

Posted on April 04, 2018 at 08:54

Thank you!

Issue sovled!

Raivo

Thomas Miehle
Associate
Posted on April 04, 2018 at 11:30

Thank you, this was the right workaround.

This link doesn't work