cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DH low peak to peak values (for machine vibration)

hani naanaa
Associate
Posted on March 18, 2018 at 21:35

I am using a LIS3DH to measure a machine's vibration, I understand that mems accelerometers are not usually used for this application, but nevertheless, I set up the acc to High resolution mode which gives me a bandwidth of 150Hz. I have the LIS3DH set up and comparing its data with a piezo accelerometer that I have. I noticed that at low frequency (under 40Hz) peak to peak values of both accelerometers are very similar. but when I go over that (80-100 Hz) I start to see a drop in the LIS3DH p-p compared to the other one. Is the LIS3DH just not suitable for this application ?

#lis3dh-machine
1 REPLY 1
Miroslav BATEK
ST Employee
Posted on March 19, 2018 at 15:04

What is the difference between the LIS3DH and the piezo sensor?