cancel
Showing results for 
Search instead for 
Did you mean: 

Fixed heatsink Zth

Jed Wang_O
Associate
Posted on March 20, 2018 at 15:09

0690X00000604UYQAY.jpg
1 REPLY 1
Alessio Corsaro
Associate II
Posted on March 21, 2018 at 11:23

Ciao Jed, thanks for your question!

The parameters in the red circle are related to the 4th degree Foster model fitting the heatsink thermal impedance (it is a RC network, as infigure 21 of the UM).

You have to fill the R fields with the R1,...,R4 values and the

https://wikimedia.org/api/rest_v1/media/math/render/svg/38a7dcde9730ef0853809fefc18d88771f95206c

fields with thefour time constants (

https://wikimedia.org/api/rest_v1/media/math/render/svg/38a7dcde9730ef0853809fefc18d88771f95206c

1= R1*C1,...,

https://wikimedia.org/api/rest_v1/media/math/render/svg/38a7dcde9730ef0853809fefc18d88771f95206c

4=R4*C4).

You can also set a lower degree Foster model for the heatsink thermal impedance, filling the first R-

https://wikimedia.org/api/rest_v1/media/math/render/svg/38a7dcde9730ef0853809fefc18d88771f95206c

couple (for 1st degree Foster model), the firsttwo

R-

https://wikimedia.org/api/rest_v1/media/math/render/svg/38a7dcde9730ef0853809fefc18d88771f95206c

couple (for2nd degree Foster model), or the first threeR-

https://wikimedia.org/api/rest_v1/media/math/render/svg/38a7dcde9730ef0853809fefc18d88771f95206c

couple (for3rd degree Foster model).

The thermal impedance you have set for the heatsink will be used to simulate the case temperature in all the steps (t1-t5 in your example).