2018-04-01 10:13 AM
Hello, First of all, I am sorry for my english. Then I am doing a application with CANBUS Protochol. so ı need to use PB13 pin of STM32F429. but when I use this pin, CAN2 is not work. When I look datasheet, this pin is connected VBUS. I set the pin to GPIO_AF9_CAN2, but This is not work still. Can do you help me?
2018-04-01 10:43 AM
This has to be at least the fourth thread you've opened on this same topic, please don't do that..
https://community.st.com/0D50X00009XkWXuSAN
It is not a chip level configuration problem, you need to address the current circuit already implemented on the board (STM32F429I-DISCO). ie remove parts or cut traces.
2018-04-01 02:02 PM
Thank you for your answer. but, I can not solve this problem.
2018-04-01 04:04 PM
2018-04-01 06:52 PM
You must take responsibility for your own work.
We can help with specific issues, but at board level, you need your eyes on it.
did you download the Schematic for this Circuit board ?
Do you have a microscope ? I use a boom zoom inspection microscope.