cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-F767ZI Pin Voltages are Too High

Eric Mintz
Associate
Posted on April 01, 2018 at 20:14

The pin voltages are too high on my board. The (nominal) 5V pin measures 6.8V, and the 3v3 pin measures 4.7. The board appears to be running normally.

I am powering the board via USB (CN1) JP1 is OFF. JP3 is set to U5V, All other jumpers have their original factory settings.

The board appears to operate OK. I've upgraded its firmware, and have written a simple program that blinks lights. However, I am having trouble getting USB2 communicating with my Linux box, and I worry that I have overdriven my 3V3 FTDI USB cable.

TrueStudio runs well on my computer, and downloads programs to the board without any trouble. Also, I have successfully communicated with various Arduino boards via USB/TTY connections

Can anyone please advise?  Thank you in advance.

Best regards,

Eric

2 REPLIES 2
Posted on April 02, 2018 at 14:05

>>Can anyone please advise?

Put a new battery in your multi-meter?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on April 02, 2018 at 14:27

Definitely, a new battery in the meter...