cancel
Showing results for 
Search instead for 
Did you mean: 

LSM303DLHCTR - Peak Current Consumption Issue

Gary Sugar
Associate
Posted on April 02, 2018 at 19:18

I'm using an LSM303DLHCTR in an application where I'm reading its X, Y and Z magnetometer values once per 20 ms, and have noticed that the chip seems to consume 10 mA or more of current from its 3.3V supply (VDD pin) - for a short interval of about 4 ms during each 20 ms cycle - presumably while it's doing a magnetometer ADC conversion. The 10 mA is much higher than I expected, since the data sheet says to expect only 110 microamps of current draw. Accelerometer is disabled in my application. 

Has anyone else seen this behavior? 

1 REPLY 1
Miroslav BATEK
ST Employee
Posted on April 04, 2018 at 16:15

Yes, there are peaks on the Icc, they are typical for magnetometer operation.

The value 110uA written in datasheet is average value.