cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link CLI erase

Jacek Stanaszek
Associate
Posted on April 11, 2018 at 10:52

ST-Link CLI rease another sector. 

STM32F767ZI, dual bank.

When using the commandline-switch -SE 15 st-link cli (v 3.2.0.0) reports:

ST-LINK Firmware version : V2J29S7

Connected via SWD.

SWD Frequency = 4000K.

Target voltage = 2.8 V.

Connection mode : Normal.

Device ID:0x451

Device flash Size : 2048 Kbytes

Device family :STM32F76x

Memory Sector @0x0810C000 erased

but erased sector 0x08108000.

Version 2.5.0 reports:

ST-LINK Firmware version : V2J29S7

Connected via SWD.

SWD Frequency = 4000K.

Target voltage = 2.8 V.

Connection mode : Normal.

Device ID:0x451

Device flash Size : 4095 Kbytes

Device family :STM32F76x

Memory Sector @0x0810C000 is not erased. Verify the memory protection.

Bank2 erase can resolve this problem.

0 REPLIES 0