2018-05-20 12:14 PM
I have a client/server LWIP program that works correctly with unicast communication however I want to use multicast features so I used IGMP library did the following:
1- in opt.h:
&sharpdefine LWIP_IGMP 1 //allowed IGMP2- in ethernetif.c:
netif->flags |= NETIF_FLAG_IGMP; //in low_level_init function
3-in my source file (for both client and server projects):
implemented the following code:
void
recCallBack
(void){ printf('connected'); //BREAK_POINT}static void UDP_Multicast_init(void *arg){ struct ip4_addr ipgroup, localIP; struct udp_pcb *g_udppcb; char msg[] = 'hello'; struct pbuf* p; p = pbuf_alloc(PBUF_TRANSPORT,sizeof(msg),PBUF_RAM); memcpy (p->payload, msg, sizeof(msg));IP4_ADDR(&ipgroup, 224, 0, 1, 129 ); //Multicast IP address.
IP4_ADDR(&localIP, 192, 168, 1, 2); //Interface IP address &sharpif LWIP_IGMP s8_t iret = igmp_joingroup((ip4_addr_t *)(&localIP),(ip4_addr_t *)(&ipgroup)); &sharpendif g_udppcb =( struct udp_pcb*) udp_new(); udp_bind(g_udppcb, &localIP, 319); //to allow receiving multicast udp_recv(g_udppcb, recCallBack,NULL); //recCallBack is
the callback function that will be called every time you receive multicast udp_sendto(g_udppcb,p,&ipgroup,319); //send a multicast packet}void telnet_shell_init(void)
{ sys_thread_new('TELNET', UDP_Multicast_init, NULL, DEFAULT_THREAD_STACKSIZE, osPriorityAboveNormal); }The result: all the mentioned code steps are executed successfully in both projects (client and server) but I'm not receiving any multicast messages (or maybe not even sending)!
I added a '
BREAK_POINT' in the callback function but I never reached it. Can you help me? either by suggesting a solution or at least a way to track the problem... I'm using STM32F746 Nucleo board with LWIP, FreeRTOS libraries generated by cubeMX.
Thank you.#freertos #lwip #udp #stm32f7-nucleo #multicast2018-08-09 09:24 PM