2018-04-24 02:08 AM
Hello,
I'm trying to export an example project for the STM32F429I-EVAL1 (to work on it).
The example works fine but when I export it :
- Either I get all the directories and the .c files BUT no includes at all
or
- I get all the directories but no files at all.
I know that it's using links from the .cproject (& .project) but I just want to dissociate the project from the rest of the examples so that I can work on it separately. (and not have all those directories at the root of my working folder like it's the case in the cubemxf4 folder).
Edit : I'm using Atollic TrueStudio to work (and do the exports)
Thanks for your help
Jules
#example #stm32f429i-eval1 #includes #export2018-04-24 05:34 AM
It looks like the problem exists since 2016 but never fixed.
2018-04-24 08:13 AM
Atollic's import/export of projects into it's 'workspace' has been a nightmare for longer than that, perhaps it is an Eclipse thing?
On Keil I can just clone projects into different directories, paths are relative, and project files in XML/ASCII so can edit them, or automate.
2018-04-24 08:18 AM
I have to, I'm adviced to use Atollic so I'll have to find a way using that beautiful IDE
🙂
.Maybe I could use Eclipse source code and import it into Atollic ?
Their way (STM) of including files / linking files is pretty good to reduce the size of the zip file but terrible for us, users.
May I import from Keil to Attolic then ?
2018-04-25 04:04 AM
CubeFW packages uses project files for SW4STM32 (can be read by TrueSTUDIO) using linked resources. As you correctly stated this is to reduce the size of the zip-file.
Eclipse/CDT in general does not have a way of importing and resolving these files into a self-contained project. Sometimes it works to export and have the c-files resolved. But the h-files are not explicitly defined by the .project file hence the knowledge of which h-file dependencies exist actually depends on each build configuration in the project.
In summary, this is a bit tricky.
2018-04-25 05:06 AM
Exactly, I imported all the .c files but have trouble finding .h / linking them . I guess that has to be done anyways.
Also I've read somewhere that it's not like that for projects generated by CubeMX nowadays, maybe someone has any infos on this?
2018-04-25 06:59 AM
I see.
Is there any way I could use CubeMX to generate again the example ?
I just finished including all the files (.c & .h) and everything works fine for now so I guess it no more is a problem for me but if it could help someone else !
2018-04-25 07:37 AM
Include files are typically pulled at compile time via search using Include Path settings. Some tools will generate a dependency tree/list in the output directory.
2018-04-25 08:00 AM
Yes, if the project is generated by CubeMx it is not a problem those projects (at least in the latest couple of versions) are generated self-sustaining. But the example projects in the Cube repo are still not. Two different use cases.