cancel
Showing results for 
Search instead for 
Did you mean: 

Stacking IHM06A1

Ciaran Bannon
Associate
Posted on May 14, 2018 at 11:29

I'm hoping someone can provide a straight-forward answer as to how I can operate multiple stepper motors using stacked IHM06A1 boards. In example code, the STSpin220 class is initialised as

motor = new STSpin220(D2, D8, D7, D5, D10, D3, PWM_REF_PIN);

Is there a simple way of declaring two 'motors' in this way, perhaps with a small hardware mod?

Thanks

#stepper-motor #stspin220 #ihm06a1
0 REPLIES 0