cancel
Showing results for 
Search instead for 
Did you mean: 

newest cubeMX (4.25.1) can not be install on macOS high sierra(10.13.3)

Rock Deng
Associate III
Posted on May 11, 2018 at 02:48

It seems that newest cubeMX (4.25.1) can not be install on macOS high sierra(10.13.3). Does any old version works? and please fix the issue of 4.25.1.

1 ACCEPTED SOLUTION

Accepted Solutions
john doe
Lead
Posted on May 15, 2018 at 00:30

its quarantined by the operating system because the st developers dont know how to sign their installers.

try this:

sudo xattr -r -d com.apple.quarantine /path/to/the/installer.app

View solution in original post

9 REPLIES 9
Imen.D
ST Employee
Posted on May 11, 2018 at 12:18

Hello

deng.rock

,

Do you mean '

cubeMX (4.1) can not be installed on macOS high sierra(3)

' ?

Best Regards,

Imen.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Nawres GHARBI
ST Employee
Posted on May 11, 2018 at 14:50

Hi

deng.rock

‌,

I tested the 4.1 install on MAC high sierra 4 and it is working fine.

Could you please launch the install in command line and give me the log

john doe
Lead
Posted on May 15, 2018 at 00:30

its quarantined by the operating system because the st developers dont know how to sign their installers.

try this:

sudo xattr -r -d com.apple.quarantine /path/to/the/installer.app

Posted on May 15, 2018 at 00:29

Sorry for my poor english. I'v already corrected that.

Posted on May 15, 2018 at 00:31

Thank you very much. I will test it again and again.

Posted on May 15, 2018 at 00:47

It replied '

xattr: No such file: /path/to/the/installer.app

'. Should I have to install or configure something before? 
Posted on May 15, 2018 at 03:04

After updated macOS to version 10.13.4, the issue still exists.

When I double clicked SetupSTM32CubeMX-4.25.1 to implement the install process, it pop up a message that shows

SetupSTM32CubeMX-4.25.1� is an application downloaded from the Internet. Are you sure you want to open it? '

and I choose open it, but nothing happened.

It seems like John doe said, the application was 

quarantined by OS. Maybe I should configure something on macOS before installation.

Posted on May 15, 2018 at 15:55

replace /path/to/the/installer.app with the path to the installer.  sorry, i thought that was obvious.

Posted on May 21, 2018 at 06:48

Thank you very much!!! Issue solved.