cancel
Showing results for 
Search instead for 
Did you mean: 

DISCO-F413ZH + X-NUCLEO-IKS01A2 Motion MEMS and Environmental sensors interrupts

Emilio Coronado
Associate
Posted on May 13, 2018 at 10:40

I recently got a DISCO-F413ZH + X-NUCLEO-IKS01A2 Motion MEMS and Environmental Sensor, and going through the example on MBED5 here: 

https://community.st.com/external-link.jspa?url=https%3A%2F%2Fos.mbed.com%2Fteams%2FST%2Fcode%2FX_NUCLEO_IKS01A2%2F

  The example code goes well partially, i can get readings through asynchronous calls, like get-xxx , etc.  However the interrupts assigned to D4, or D5 seems not being triggered, so that code does not work ? so far did not touch the board, or the header pins, same for the original code ?  do i miss something ? like enabling interrupts, pin assignments, board + header incompatibility, etc ?

#disco-f413zh-x-nucleo-iks01a2 #disco-f413zh
0 REPLIES 0