cancel
Showing results for 
Search instead for 
Did you mean: 

Boot0 Pin

Huy Nguyen
Associate II
Posted on May 30, 2018 at 06:41

what happen if I don't push the boot0 pin on Vdd or pull it to Vss, just let it float ?

4 REPLIES 4
Artur IWANICKI
ST Employee
Posted on May 30, 2018 at 07:52

Hello,

In such a case state of BOOT0 pin will depend on the external conditions. It can 'catch' some disturbances and be either 'H' or 'L' state. Thus it may happened that MCU will not start from internal FLASH (Boot0='L') but it will try to run from system memory (built in bootloader) or internal SRAM. Thus I would strongly recommend to fix the level on this pin during startup process of the MCU.

Best regards,

Artur

T J
Lead
Posted on May 30, 2018 at 07:55

run a 1k - 10K to ground for normal operation.

Posted on May 30, 2018 at 09:10

 ,

 ,

Thank you so much !

2018-05-30 12:56 GMT+07:00 T J <,st-microelectronics@jiveon.com>,:

STMicroelectronics Community

<,https://community.st.com/?et=watches.email.thread>,

Re: Boot0 Pin

reply from T J

<,

MCUs Forum* - View the full discussion

<,https://community.st.com/0D70X000006Ss7wSAC

Posted on May 30, 2018 at 10:00

Huy Nguyen wrote:

Thank you so much ! 

https://community.st.com/0D50X00009bMM5DSAW