cancel
Showing results for 
Search instead for 
Did you mean: 

Can't debug with J-LINK in Atollic Truestudio

X YK
Associate
Posted on June 05, 2018 at 15:59

hello there

   I'm new in Atollic Truestudio and i want to use j-link to debug. The problem is that when i click the DEBUG button,  its told me that there is an error with runing GDB service,pleasr check the probe's  priority setting. emmmm .That's roughly what it means(i translate the warnning notice form chinese).Then, there is a windows to let me do some configuration.just as the following picture .I have used keil 5 to develop stm32 until now,i had never seen the same setting like this , so could you please help me

solve this problem ? thanks a lot!

0690X0000060BXUQA2.png

#atollic-turestudio #j-link
2 REPLIES 2
AvaTar
Lead
Posted on June 05, 2018 at 16:18

Have you installed the drivers, i.e. the Windows USB drivers ?

The Hardware Manager should show something like this, assuming you use Windows:

0690X0000060L7yQAE.png
Posted on June 05, 2018 at 16:37

Yes,I use widows.  I had installed the j-link  drivers and I could use it well in Keil-Mdk ,but it's not work well in atollic truestudio ,I suspect it’s a problem with my setting